This project demonstrates an USB Audio Device, FFT Processing and 
FFT Result (UART)

The USB Audio Device is recognized by the host PC running
Windows which will load a generic Audio driver and add a
speaker which can be used for sound playback on the PC.

The FFT data was processed each frame and the result was sent back 
to PC via UART. 

/*************************************************************************/

Project has been tested with LPCXpresso ver 4.0.6 and ver4.1

Please follow the instructions in the Application Note to setup and debug.
When the program is flashed on to the target and all other instructions are followed as mentioned in the Application note, 
the LED on the board will be blinking continuosly. 
If The LED is not blinking and is continuosly switched on, then it indicates and error indicating that the USB Audio (J8) is not plugged in.
For more details refer the Application note.